Other Parts Discussed in Thread: AM1808, OMAP-L138
Hi,
I am working on an AM1808 based custom board we designed (inspired from Hawkboard + AM1808 evm from LogicPD).
We have a nand memory : MT29F8G08ADBDAH4 which seems to be working :
We are able to boot from UART (using AISGen + OMAP-L138 UART Boot Host utility) and launch u-boot
In here, we are successfully able to play with the nand memory (nand erase/write/read works and data is still there after a hard reset).
We have been generating a u-boot AIS-signed for NAND boot and trying to write it to block 1 of nand, but after reset (and the correct boot mode selected), we were unable to see u-boot console.
--> in u-boot :
tftp C0700000 u-boot_nand.ais (u-boot_nand.ais is 190KB)
nand erase 20000 40000
nand write C0700000 20000 40000
...then power cycle the board in nand boot mode...
We did that exact same procedure, with the exact same u-boot file on our hawkboard which booted correctly (we have the same DDR2 as in the Hawkboard.
We have also done the exact same procedure on our AM1808 EVM with the same u-boot (but AIS signed for the EVM, which have an mDDR...), it booted successfully from nand.
We have also been trying the Serial boot and flash loading utility for OMAP-L138 (http://processors.wiki.ti.com/index.php/Serial_Boot_and_Flash_Loading_Utility_for_OMAP-L138), which works perfectly with our EVM (still with the same signed u-boot file)
We have been able to customize it (the SFH utility) and recompile for our board (wa have a DDR2 memory). with this, it worked well with the Hawkboard but not with ours : the utility fails to write our nand memory.
Could anyone enlighten us ? Is there something we missed ?
Thanks in advance.
Veranith