This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: QSPI DAC mode

Part Number: AM6442


Tool/software:

Hi Expert,

customer is using VxWorks os, and they want to enable the DAC mode, but they find some mismatch between the input and output, they have some debug as below:

This problem we take data analysis, is while writing flash, although we wait for the ospi _cfg (0x0) register bit31 bit bus to be idle, but the actual data is not sent out. Then another packet comes in, sending 50 cm clear. So does this bit of such a bus idle really mean that the data is sent? Are there any other status bits to indicate? To make sure that my data is sent on the next shot.

Can you help answer customer question?

BR,

Biao