TPA3112D1: Clarification on “Output Differential Duty-Cycle” in TPA3112D1 DC Detect

Guru 12175 points
Part Number: TPA3112D1

Tool/software:

Hi,

I am referring to the TPA3112D1 datasheet, section 7.3.5 DC Detect, which states:

- A DC Detect Fault is issued when the output differential duty-cycle exceeds 14% (for example, +57%, -43%) for more than 420 ms at the same polarity.

Could you please help clarify the definition of “output differential duty-cycle”?
The datasheet provides waveform examples, but it is not explicitly labeled. I would like to confirm whether the following interpretation is correct:

  • It refers to the deviation of the average differential voltage across the load (OUTP−OUTN), determined by the duty-cycle difference of the OUTP and OUTN switching waveforms.

  • For example, if OUTP=57% and OUTN=43% continuously for more than 420 ms, a DC Detect Fault will be triggered.

Could you please confirm if this understanding is correct?

Thanks,

Conor

  • Hi Conor,

    Your understanding is correct, the output differential duty cycle refers to the difference in duty cycle between OUTP and OUTN switching waveforms.

    If this duty cycle difference exceeds 14% for more than 420ms, a DC detect fault will be triggered. Is this clear?

    Best regards,

    Sebastian