Part Number: TDA4VM
Tool/software:
Hello Team,
I have a video pipeline application which makes use of tensorflow model and the algorithm has dependencies on OpenCV. Can you please guide in porting this application into TDA4VM?
Best Regards
Chethan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
Tool/software:
Hello Team,
I have a video pipeline application which makes use of tensorflow model and the algorithm has dependencies on OpenCV. Can you please guide in porting this application into TDA4VM?
Best Regards
Chethan
Hello;
Thanks for the question.
For video pipeline application development, please refer to this link.
You can build the demo examples that come with SDK first. Depend on your application, you can modify the examples accordingly.
For Tensorflow; please refer to this link:
https://github.com/TexasInstruments/edgeai-tidl-tools
You can git-clone the TIDL edgeAI tool.
We recommend to use ONNX format, then import your ONNX format model to TIDL flow.
If you already have a TI EVM, your can verify the model inference on the EVM in real time, and test the vision apps in real time as well, including camera/image-sensor and display in your pipeline.
Best regards
Wen Li
Hello,
The engineer assigned is currently out of office. They will return beginning of next week and will be able to update. We appreciate your patience.
Warm regards,
Christina
For the model compiling guideline:
1. Please create a model instantiation in the "model_configs.py"; this is the file in the downloaded edgeai-TIDL-TOOLS folder, under the "../examples/osrt_python/" sub-folder.
2. I am using the yolo model as an examples and paste below. You should config your file with the parameters that fit your model&Application
3. There is another "common_utils.py" file, please adjust the parameters according to your model as well.
Then you can compile or inference your model.
Here are the commands to compile and inference a model
1. Compile and inference a model
python3 onnxrt_ep.py -c -m yolox_s_pose_ti_lite
2. Inference a model only
python3 onnxrt_ep.py -m yolox_s_pose_ti_lite
=======================================================================================
"od-8200_onnxrt_coco_edgeai-mmdet_yolox_nano_lite_416x416_20220214_model_onnx": create_model_config(
task_type="detection",
source=dict(
model_url="">software-dl.ti.com/.../yolox_nano_lite_416x416_20220214_model.onnx",
meta_arch_url="">software-dl.ti.com/.../yolox_nano_lite_416x416_20220214_model.prototxt",
infer_shape=True,
),
preprocess=dict(
resize=416,
crop=416,
data_layout="NCHW",
pad_color=[114, 114, 114],
resize_with_pad=[True, "corner"],
reverse_channels=True,
),
session=dict(
session_name="onnxrt",
model_path=os.path.join(
models_base_path, "yolox_nano_lite_416x416_20220214_model.onnx"
),
meta_layers_names_list=os.path.join(
models_base_path, "yolox_nano_lite_416x416_20220214_model.prototxt"
),
meta_arch_type=6,
input_mean=[0, 0, 0],
input_scale=[1, 1, 1],
input_optimization=True,
),
postprocess=dict(
formatter="DetectionBoxSL2BoxLS",
resize_with_pad=True,
keypoint=False,
object6dpose=False,
normalized_detections=False,
shuffle_indices=None,
squeeze_axis=None,
reshape_list=[(-1, 5), (-1, 1)],
ignore_index=None,
),
extra_info=dict(
od_type="SSD",
framework="MMDetection",
num_images=numImages,
num_classes=91,
label_offset_type="80to90",
label_offset=1,