This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H14: Tx driver equalization

Part Number: 66AK2H14

Tool/software:

Hi Community,

I would like to understand the Serdes Tx parameters based on the spruho3b document.

§14.2.3 declares 4 parameters C0,C1,C2,CM where C0 is calculated from the CM,C1,C2 values. Equation (3) gives a relation between those values

And Indeed CM,C1,C2 can be adjusted by manually adjusted by software (registers do exist)

But in the same paragraph we can see another formula where C0+C1+CM = 1 (normalization) without any reference to C2. It is therefore explained that C0 only depends upon C1, CM and not C2

Could you explain please ?

In figure 14 we can see de-emphasis, preshoot and boost calculation but nothing depends on C2 value ! So what is the purpose of C2 then ? This is quite confusing 

If you could give some explanations it would be great.

With best regards,

Bruno

  • Hi,

    The assigned engineer is out of office today. Expect response early next week.

    Thanks,
    Keerthy

  • Hi Bruno,

    Apologies for the delay and Thanks for the patience.

    As mentioned in KeyStone II Architecture Serializer/Deserializer (SerDes) - User Guide, the transmitter utilizes a 4-tap FIR filter with coefficients Cm, C₀, C₁, and C₂.

    Then the output can be expressed as: 

    y(n) Cmdn+1+C0dn+C1dn1+C2dn2

    The coefficients Cm, C₀, C₁, and C₂ can be positive or negative, based on the lane control register bits.

    And the normalization condition here is as follows:

    (Normalization Eq:1 - Generic Mode) ∣Cm+C0+C1+C2=1

    As the values of Cm, C₁, or C₂ are increased, C₀ is automatically decreased to maintain this equality.

    from the above screenshot, it is mentioned that "The equalization ratios implemented by the transmitter can be calculated from the PCIe tap-coefficients in PCIe mode or register settings in generic mode."

    In PCIe mode, the SerDes usually supports post-cursor de-emphasis (C1) and main cursor (CM). In those modes, The C2  (pre-cursor tap) effectively not utilized /is set to zero.

    Therefore, the normalization simplifies to:

    Cm + C0 + C1 = 1 ( Eq:2PCIe equalization case, where only Cm and C1 are relevant.)

    In Section 14.2.2 : " PCIe mode, TX driver equalization and swing/slew settings are controlled by a Look-Up table (LUT). For any reason, if these setting need to be controlled through registers then the override enable must be asserted"

    Regards,

    Betsy Varughese

  • Thank you Betsy for your answer.

    Sorry, I did not mention that my application was not PCIe but 10G-XFI.

    Therefore I did not really consider the 14.2.2 § which do focus on PCIe

    therefore it was not obvious that the calculation example chosen in § 14.2.3 (which I consider as a generic explanation) was actually oriented to PCie.

    Then for 10G you confirmed that C2 was involved in the  TX waveform (at the condition that override is asserted).

    Is this correct ?

    with best regards,

    Bruno

  • Hi Bruno,

    Could you please go through the document https://www.ti.com/lit/an/sprac37/sprac37.pdf?, I believe it will be helpful in addressing this query.

    Regards,

    Betsy Varughese

  • Hi Betsy,

    Can you explain how the Override can be achieved?

    The spruho3a (last version from July 2016)  table 14-2 says that OVR controls can be found at address LANE_0A8, LANE_0A0

    but these address do not exist 

    Can you precise please ?

    regards,

    BRuno

  • Hi Bruno, 

    I don't think its a CPU memory mapped address, Instead It is the offset inside the SerDes lane register space. 

    You can find the memory map details in Chapter 16 of https://www.ti.com/lit/ug/spruho3a/spruho3a.pdf?.

    Regards,

    Betsy Varughese

  • Hi Betsy,

    I am not sure to understand your comment.

    I was precisely referring to the spruho3a document ! and precisely the Serdes lane register space.

    LANE_0A0 and LANE_0A8 are defined as "reserved"

  • Hi Bruno,

    LANE_0A0 and LANE_0A8 are defined as "reserved"

    Could you please check this? , For PHY-A, those lane's are not reserved.

    Yes, If you are working with PHY-B, in that case the configuration is “reversed.”

    Regards,

    Betsy Varughese

  • Hi Betsy,

    It seems that your picture corresponds to PHY-A serdes mapping (table 16-1)

    For 10G which is our use case we have to look at PHY-B table (see my previous snapshot extracted from table 16-2)

    Don't you agree ?

    Regards,

    Bruno

  • Hi Bruno,

    Yes I have updated the comment. 

    The spruho3a (last version from July 2016)  table 14-2 says that OVR controls can be found at address LANE_0A8, LANE_0A0

    This table actually describes about the "Register Descriptions for PCIe Mode TX Driver Slew, Equalization and Amplitude Settings".

    For Generic Mode, Please refer the below table.

    Table 14-4. details about the "TX Driver Register Signals for PHY-B".

    Regards,

    Betsy Varughese