Other Parts Discussed in Thread: AM3517
Hello,
I am getting some performance issues with USB function controller on omap3x series processors. I am getting 41Mbps throughput with modem class and 27Mbps with mass storage class. I have tried the tests on Beagle (OMAP35X), AM3517EVM and Beagle XM (OMAP37X) and get the performance issues with all these processors. These platforms have MUSBMHDRC USB OTG IP.
Does anyone have numbers on Linux for USB function controller for OMAP3X platforms? or experienced the performance issues with OMAP3X USB function controller.
Thanks