AM6442: Is it possible to include OTP key writer in boot media such as eMMC?

Part Number: AM6442
Other Parts Discussed in Thread: AM62P

Tool/software:

Hi,

Now customer is investigating where they should store OTP keywriter.

If they store OTP keywriter other media than boot media, they might be asked to verify security risk for the media of OTP key writer to follow CRA.

Here is the question.

  1. Is it possible to include both OTP keywriter together with boot loader, RTOS and Linux rootfs? When boot up 1st time, OTP keywirter runs and program keys. 2nd time or after, boot Linux and RTOS runs. Is it possible to support this use-case?
  2. As another way, is it possible to program keys in OTP using JTAG? After OTP is programmed, JTAG is disabled, so there is no security risk for the path to program OTP keywriter.  This is ideal case for customer. After that, only boot loader, RTOS and Linux runs.

Best Regards,

Kasai