This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Wake up fuctionality implementation in DM8148 through USB HUB.

Other Parts Discussed in Thread: TUSB2046B

Hi ,

One of my customer is developing Thin client application based on DM8148 processor , please do find the below query & get back to me with your valuble feedback.

a) The DM8148 has 2.0 two USB port with wake up fuctionality ?  if it so DM8148 USB port will support the TUSB2046B USB HUB with wake up fuctionality ?

b)  DM8148  has internal temp sensor to monitor the  Temp of DM8148 ?

Regards/

vengat

  • Hi,

    a. This reply is from USB Peripheral operation perspective not from the Device (System) level perspective. We do support a capability of waking up from SUSPEND state. Also in an OTG envirnoment, an OTG device device can wake up the USB using SRP protocol. Other than these two methods, I am not aware of a special h/w that is implemented at the device level to perform any other type of wake up mechanism. I will ask the USB PHY experts for any other type of functionality implemented.

    b. I will let others address this question.

    Best regards, Zegeye