Part Number: TDA4VM
Tool/software:
Hello TI,
I've a question related to the SDL APIs for the CCM module, I see here for example the API "SDL_CCM_init" takes a parameter of the type "SDL_CCM_Inst" as an input, but when I checked this type for the main domain r5f cores I found that only supported cores are the SDL_CCM_R5F0 and the SDL_CCM_R5F1 but SDL_CCM_R5F2 is not defined here, so my question is is it supported or not? and if not then is it planned to be supported in ay other later versions? if yes then when is it expected to be delivered?
Thanks in advance.