This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7: AM62A7: TIOVX The outputs of the segmentation model from board and ONNX are inconsistent.

Part Number: AM62A7


Tool/software:

Hello,   

I am currently running a segmentation network on the AM62A7 board,  The model compilation was successful, and the model forward on the board is also functioning normally, however I met a problem, that is  the outputs of the segmentation model  from board inference and ONNX inferrence are inconsistent.

My current edgeai_tidl version is edgeai-tidl-tools-10_01_03_00. ,I used the onnxrt_ep.py script to compile the onnx model, resulting in io_1.bin and net.bin , the compile log save in the model_compile_log.txt 

I will provide you with my onnx model, the compiled binary files, and the compilation logs,  model_configs.py and common_utils.py 8267.attachment.zip. May I ask what this issue is? I hope to receive your answer, thank you very much.

Best wishes

zhuang yihao