Part Number: J721EXCPXEVM
Tool/software:
Hi,
We are using the J721EXCPXEVM with the J7200XSOMXEVM for our proyect development.
We would like to know if it is possible to use the WKUP-UART0 to print all the boot logs and the u-boot terminar and also the terminal of linux. What are the steps to configure this?
I would like to use this wkup-uart in the way the MAIN-UART0 is alredy configured.
Im using the ti-processor-sdk-linux-j7200-evm-11_00_10_01.