This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 example/test code for USB, SD, HDMI, video capture



I am looking for test/example code for the DM8168 that can simply be run within Code Composer Studio. Spectrum supply several tests for the EVM in their evm816x_BSL.zip archive, but only basic tests for DDR3, Audio, EMAC, SATA, UART ,I2C etc.

The tests I'd like to find are:

1) Video capture,

2) HDMI output,

3) SD card, and

4) USB host.

 

The 1st is probably too complicated for a Code Composer Studio environment, but is there a non-Linux HDMI test (i.e. something that can be run under CCS)?

And any SD card or USB host test/examples would also be useful.

Thanks.