This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

need help migrating to a newer kernel



I'm maintaining a 2 year old project based on linux-omap-psp 2.6.32 kernel and gstreamer-ti on a gumstix

I'd like to update to a newer kernel.  I've settled out on linux-omap3 2.6.39, mostly because I had too much trouble getting the 3.0.* kernels up and going.

I'm also hopelessly mired in the oe-classic vs oe-core split that seems to have happened.

I've decided to stick with oe-classic, and I've got a recipe for linux-omap3 2.6.39 that compiles and boots, but I'm having trouble getting the gstreamer bits up to date.

I've found conf/distro/include/angstrom-codec-engine-latest-preferred-versions.inc , which seems to specify versions of various TI bits to use.  I've changed my PREFERRED_VERSION_ti-linuxutils = "3_21_00_04" (and created a new recipe for that) to match the kernel version, and get the CMEMK module working.  I suspect other things in there need changing, but I'm not sure what, or what they need changing to.

When I "gst-launch playbin2 uri=rtsp://foo" I get :

ERROR: from element /GstPlayBin2:playbin20/GstPlaySink:playsink0/GstBin:vbin/GstAutoVideoSink:videosink/GstOmapFbSink:videosink-actual-sink-omapdmaifb: failed to create dmai framecopy handle

Additional debug info:

omapfb.c(523): x_memcpy (): /GstPlayBin2:playbin20/GstPlaySink:playsink0/GstBin:vbin/GstAutoVideoSink:videosink/GstOmapFbSink:videosink-actual-sink-omapdmaifb:

failed to create dmai framecopy handle

Am I doing this the hard way? How can I find a holistic set of TI stuff to use in conf/distro/include/angstrom-codec-engine-latest-preferred-versions.inc ?