Part Number: J784S4XEVM
Other Parts Discussed in Thread: TDA4VH
Tool/software:
I received the attached lauterbach scripts from Richard Woodruff before and have some questions about it. I am using it to load my app to R5F core.
1: Is there a scripts that touch R5F, assuming that all other necessary configurations are already done by firmware/device manager/u-boot ?
2: The scripts is assuming the EMU0/EMU1 are used and have been at required state. In our customized board, we are not using EMU0/EMU1, we need bypass EMU0/EMU1 state check
3: Why do we need run this baremetal setup ? How could we skip this scripts if we don't need touch flash memory?
; Setup for GP or HS {HS:FS, HS:SE}
DO "&path/../_J784S4_baremetal_setup.cmm" HS:FS
4: why do we need run _J784S4_m4.cmm for r5f core ? could it be skipped ?
; Attach to M4 to start SOC bring up
TITLE "TRACE32 for ARM - J784S4-CM4 - MASTER" ; set GUI title
DO "&path/../_J784S4_m4.cmm" CM4-0 PREPARE
5: Those clock configuration should be covered by u-boot. Could this scripts be skipped ?
; From M3 initialize clocks and install global functions
DO "&path/../J7AHP.cmm" DMSC_FLOW
Thanks