This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62L: AM62L: Unable to wake from sleep(The GPIO in the WAKEUP domain )

Part Number: AM62L


Tool/software:

Hi,

Referencec: https://software-dl.ti.com/processor-sdk-linux/esd/AM62LX/11_00_15_05/exports/docs/devices/AM62LX/linux/Release_Specific_Release_Notes.html

Using the device tree: k3-am62l3-evm.dts. Executing the command "echo mem > /sys/power/state" fails to wake up effectively via wakeup_uart. Could the GPIO in the WAKEUP domain be used to wake up the DeepSleep state? This includes: WKUP_GPIO0_0, WKUP_GPIO0_1, WKUP_GPIO0_2, WKUP_GPIO0_3, WKUP_GPIO0_4, WKUP_GPIO0_5, and WKUP_GPIO0_6. If it is possible, how should it be adapted?