Tool/software:
Hi Team,
- We designed a board using the processor TMS320DM8168CCYGA2 (nearly 10 years ago) and the board is in production. Recently we built 40 boards.
- Out of those 40 boards, on one board we are facing an issue while uboot flashing. Rest 39 boards are flashed successfully without any issue.
- When we try to flash the processor through Code Composer Studio, we first load the NAND writer setting file. At that instant, CCS reports a data verification error at address 0x80000003. In 39 boards, the same GEL file and NAND writer binary load successfully and NAND flashing works.
- Our question is: Why does CCS report a verification error at address 0x80000003 during NAND writer file load?
- I have also attached the screenshot of the error.
We would appreciate your guidance on resolving this issue. Looking forward to your helpful response.
Environment
Processor: TMS320DM8168CCYGA2
External RAM: MT41K128M16JT-125 IT: K (DDR3)
Version: CCS Version: 10.1.1
JTAG Probe: Texas Instruments XDS100v2 USB Debug Probe
Already checked below things:
- We have already checked and compared all the power rails, clock signals and reset lines in the faulty board – everything looks fine.
- We replaced the DDR termination resistors. Later we replaced DDR device too.
- We replaced the series resistors of JTAG & EMU interfaces.