This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VEN-Q1: Regarding the setup of TDA4VEN MCAL/examples based on FreeRTOS

Part Number: TDA4VEN-Q1
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

Hi

SDK 11.0      domain: MCU

Regarding the setup of TDA4VEN MCAL/examples based on FreeRTOS:

  1. We downloaded MCUSW_J722S_11.00.00.05 from the J722S SDK download page and copied the MCUSW to the SDK directory ti-processor-sdk-rtos-j722s-evm-11_00_00_06/. We also modified the paths for sysconfig and CCS as shown in the figure.

  2. After completing the path modifications, we ran make can_app -j16 in the directory ti-processor-sdk-rtos-j722s-evm-11_00_00_06/mcusw/build. The compilation was successful, and the program could run normally via an SD card.

Under the above conditions, we now want to set up FreeRTOS in ti-processor-sdk-rtos-j722s-evm-11_00_00_06/mcusw/mcal_drv/mcal/examples/Can. During the setup process, we encountered many issues. Therefore, we would like to ask if there are any reference examples available for guidance?

Best regards

Bingxian

  • Hello,

    In MCU+SDK , there are no freeRTOS based examples in MCUSW. May i know why MCAL examples are being used with freeRTOS rather than AUTOSAR OS ?

    If you require freeRTOS examples , we have it in MCU +SDK rather than MCUSW.

    Regards

    Tarun Mukesh