This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Camera interface on beagleboard-XM (Rev C) + Gingerbread

Hi, 
I'm encountering a problem using camera interface on beagleboard-XM (Rev C) with android gingerbread .I've downloaded the Pre-Build image and source
from TI website :
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_tii/TI_Android_DevKit/TI_Android_GingerBread_2_3_4_DevKit_2_1/index_FDS.html

And then I have followed the steps of User Guid to make SD card. When I clipped the Camera icon - (Application->Camera),and after I waited a long time, I've got
a error message on the screen : Activity Camera (in Application Camera) is not responding.
The camera sensor I've used is MT9V113.

The attached documents :

1.Booting log from the serial console

 2.logcat log

Thank you !

7115.logcat.TXT2577.booting.TXT

  • Hi Zhong,

    1. Similar question has been posted to rowboat googlegroup also, I am not sure it was by you or ...?

    2. From the log I can see

    - Camera is detected on boot. But while setting up media link it is failing

    See logs - "Failed to setup media link....."

    Could be several reasons for the same

    - connection is not proper

    - sometime rebooting the device will correct the proplem, as media links gets reset on boot

    3. Have you  modified any thing in kerenl? If yes can we know what changes have you done for the same

    4. Also give dmesg while opening camera app.

    BR,

    satish