This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320Vc5509A jtag problem

Hi;
my problem is when I am connecting to TMS320VC5509A;the following error message is appearing:
Error connecting to the target:
Error 0x80000242/-1143
Fatal Error during: Memory, Initialization, OCS,
The memory at 0x000000BE continually indicated it was 'not ready'
All memory operations currently in progress were aborted in order
to regain control of the processor.
This is considered a catastrophic event, but the debugger should
still be able to access memory and CPU registers.
System state has been altered. It is strongly advised
that the processor should be reset before resuming execution,


Sequence ID: 0
Error Code: -1143
Error Class: 0x80000242
I/O Port = 0

Board Name: Blackhawk USB510L- C55xx Emulator
Cpu Name: TMS320C5500_0

Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.


Regards;
Ipsit