This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 EVM setup script u-boot parameters not working



I just installed ti-ezsdk_dm814x-evm_5_03_01_15 and ran the setup script. It eventually says:

Resulting u-boot variable settings:

setenv bootdelay 4
setenv baudrate 115200
setenv bootargs console=ttyO0,115200n8 rootwait rw mem=256M earlyprintk notifyk.vpssm3_sva=0xBF900000 vram=50M ti814xfb.vram=0:16M,1:16M,2:6M root=/dev/nfs nfsroot=192.168.0.136:/srv/dm814x-evm/filesystem ip=dhcp
setenv bootcmd 'colorbar;dhcp;setenv serverip 192.168.0.136;tftpboot;bootm'
setenv autoload no
setenv serverip 192.168.0.136
setenv bootfile uImage-dm814x-evm.bin

When I use those parameters in u-boot I get the following:

Net:   <ethaddr> not set. Reading from E-fuse
Detected MACID:40:5f:c2:40:97:ec
cpsw
Hit any key to stop autoboot: 0
Unknown command 'colorbar' - try 'help'
link up on port 0, speed 1000, full duplex
BOOTP broadcast 1
DHCP client bound to address 192.168.0.122
link up on port 0, speed 1000, full duplex
Using cpsw device
TFTP from server 192.168.0.136; our IP address is 192.168.0.122
Filename 'pxelinux.0'.
Load address: 0x81000000
Loading: T
TFTP error: 'File not found' (1)
Not retrying...
Wrong Image Format for bootm command
ERROR: can't get kernel image!
TI8148_EVM#

It would appear that calling 'dhcp' changes the bootfile from uImage-dm814x-evm.bin to pxelinux.0

setting bootcmd to 'dhcp;setenv bootfile uImage-dm814x-evm.bin;setenv serverip 192.168.0.136;tftpboot;bootm' would appear to fix this issue.

Not sure what the colorbar is all about