This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7-Q1: LinuxAppImage authentification problem with NOR QSPI Flash

Part Number: AM62A7-Q1
Other Parts Discussed in Thread: UNIFLASH, SYSCONFIG

Tool/software:

Hello,

I am using a custom hardware using the TI AM62A7-Q1 Soc. On the board I have a QSPI NOR flash (Part Number - IS25WE256E) as well as an eMMC flash.

I am using the uniflash tool to flash the core images using the configurations as provided by TI. I can flash the images using the sbl_prebuilt/default_sbl_ospi_nand_hs_fs.cfg (ipc_rpmsg_echo_linux.release.appimage) onto our qspi nor and it works 

However when i try to flash the linux.appimage.hs_fs using the sbl_prebuilt/default_sbl_ospi_nand_linux_hs_fs.cfg, the images are flashed successfully. However on booting from QSPI i get the following error as seen below 

Bootloader_verifyMulticoreImage:619 Failed to authenticate and copy on the go, reading the image to DDR

Bootloader_verifyMulticoreImage:680 Failed to authenticate Image

 

The same linux.appimage.hs_fs works and boots perfectly when flashed onto the emmc flash

It would be great if I could get some support on this. Please let me know if further information is needed

Regards,

Nikhil