This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: QDMA

Part Number: TMS320C6678

Tool/software:

Setup:            

  • Board: EVM6678
  • SDK: Processor SDK 6.03.00.106
  • Example: Nimu_emacExample (includes NDK library and Daemon function)
  • Added module: H.265 encoder example (h265venc_ti_c66x)

Both the NIMU/NDK example and the H.265 encoder are running correctly.

Requirement:
The project needs to use QDMA to minimize memory-to-memory copy latency.

Question:
What is the recommended way to enable and use QDMA in this project, while ensuring that it does not conflict with EDMA3 LLD and Framework Components 3.40.02.07?