This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to make the same an input frame rate and an output frame rate, use a VFPC-DEI module?

Hi.

I used "OMX.TI.VPSSM3.VFPC.DEIHDUALOUT" in ti-ezsdk_dm816x-evm_5_03_01_15.

I want
Input Video port is 60fs 1920x1080 YUV420.
Output Video port 0 is 60fs 1920x1080 YUV422.
Output Video port 1 is 60fs 1920x1080 YUV420.

But, output frame rate is half of input frame rate.
Output Video port 0 is 30fs 1920x1080 YUV422.
Output Video port 1 is 30fs 1920x1080 YUV420.

DEI modues can execute same rate of input and output ?

Regards.
miki shinji