This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCI Express EP device link-up failure with ti8148 EVM

Hi,

I am using TI8148 EVM to test PCI Express End point device. The set-up is to connect the PCI Express endpoint device to the Root complex port of ti8148 EVM.

The End point device link-up is not happening and the device is not getting detected on the ti8148. The EP device is configured with X1 link.

I had made changes to the hardware for the PERST line to set as OUTPUT (default High) and i am asserting the PCIe_POR using i2c write command

as described in the PSP Root Complex Document.The kernel is build with PCI support.

Do i need to do any other setting to detect the EP device connected.

Note: The PCIe End-point device is getting detected on other X86 PCs.

Please help to resolve this issue. Is there any known issue with PCI express root complex on 8148 EVM?

Thanks and Regards,

Ansa Ahammed