This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GP timer



Folks,

I'm developing on DSP c5504 with CCS3.3 and Bios 5 .

 Timer0 is declered in my project as 1 milisec CLK ( *.tcnf)

I need to use another HW timer with a 1 microsec resolution . since tcnf allowed only one resolution to Timer0,  Timer1 and timer2 I have to implement it using CSL .

I have few questions:

1) I tried to run timer1.prj located in the ccs3.3 example but it doesn't work. have someone tried it before?

2)  tcnf using HWI_INT4 for Timer0. which I assuming i the same for Timer1 and Timer2 but I can't change the interrupt service routine implementation .

3) Is there any other examples for implementing the HW timer interrupts?

 

your help is more than appreciated ,