Other Parts Discussed in Thread: TDA4VM,
Tool/software:
I'm in the 10_01 RTOS SDK for J721e, so this applies to a number of devices, but I'm doing some testing on the TDA4VM board here.
This is a question about the usage of GPIO_DEVICE_CONFIG in the main_led_blink example.
It defines the macro with parameters (port, pin); also above it, it defines GPIO_MAX_NUM_PORTS as (2U). Am I to assume that the two ports here is meant to be WKUP domain and MAIN domain? How would MCU domain come into this?
Consider the case if I want to add a few more GPIOs to the demo. When I define the pin config, what would I use?