HI all,
I'm using CCS v5.0.23. Is profiling available for hardware EVMC6678LE????? I have done it usoing simulator. But did not find one for the hardware.
Regards,
Sohal
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI all,
I'm using CCS v5.0.23. Is profiling available for hardware EVMC6678LE????? I have done it usoing simulator. But did not find one for the hardware.
Regards,
Sohal
As per :
http://processors.wiki.ti.com/index.php/Profiler
which states :
"Note: Due to the Function Profiling feature not being very accurate on C6000 HW, support for it has been disabled in CCSv4. Alternate solutions are to use the profile clock or a trace based solution. ". So it is preferable to do profiling on simulator.
Alternately, You can Multicore system analyzer, with h/w and s/w instrumentation.
http://processors.wiki.ti.com/index.php/Multicore_System_Analyzer
Example :
http://processors.wiki.ti.com/index.php/MCSA_and_the_MCSDK_Demo
Just FYI : CCSv5.1 is now available @
http://processors.wiki.ti.com/index.php/Download_CCS