This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem displaying image using DM365

Hi ,

I successfully booted into DM365 and am able to get the ridgerun logo on a composite output . But when i try to copy an image into fb0 i dont see a change in the image at the output . Here's a list of commands i entered. Even fbset stops working after i use cp . Any help appreciated .

# fbset

mode "720x480-30"
        # D: 12.500 MHz, H: 14.863 kHz, V: 29.966 Hz
        geometry 720 480 720 480 16
        timings 80000 121 0 16 0 0 0
        accel false
        rgba 5/11,6/5,5/0,0/0
endmode

 # cp /opt/demo2/osd.r16 /dev/fb0
 # fbset
fbset: FBIOGET_VSCREENINFO: Inappropriate ioctl for device