Other Parts Discussed in Thread: PROFIBUS, AM3359
Hi,
I try to sort out whether we can use a AM335x in a new design or not. EtherCAT is a possible interface. Therefore I try to figure out which pins I therefore need.
In the Technical Reference Manual I have not found any informations about the following peripherals or feature of the PRUSS:
- MII_RT
- IEP
- MDIO
- EDIO
Is there any documentation that points out which pins are needed for certain use case (eg EtherCAT, Profibus etc., etc.)?
Any schematics of the Industrial Communications Engine (ICE) available (also beta schematics appreciated)?
Is it true that if the PRUSS is used for EtherCAT it's difficult to use the GPMC? Any applications that uses parallel Flash and EtherCAT (maybe ICE schematic would help)?
Thanks for support.
Best regards,
Patrick