This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Remoteproc state: Attached

Part Number: TDA4VM

Tool/software:

Hi,

Im using TDA4VM j721e_evm board and in this i have flashed the "tisdk-adas-image-j721e-evm.rootfs" filesystem and i not able to load my firmware through remoteproc due to the attached state im not able to stop or start the main r5f0_0 

root@j721e-evm:~# head /sys/class/remoteproc/remoteproc*/state
==> /sys/class/remoteproc/remoteproc0/state <==
detached

==> /sys/class/remoteproc/remoteproc1/state <==
attached

==> /sys/class/remoteproc/remoteproc2/state <==
offline

==> /sys/class/remoteproc/remoteproc3/state <==
attached

==> /sys/class/remoteproc/remoteproc4/state <==
attached

==> /sys/class/remoteproc/remoteproc5/state <==
attached

i have tried detaching it and stop and load the firmware im not able to load it.

Thanks

Balaji