This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

configuring two MCBSP's for two different SPI devices on DM6437

Hi,

I am on the verge of deciding my design with DM6437.

I am planning to configure one MCBSP0 for SPI flash(for booting), and the other MCBSP1 as SPI interface with FPGA. From the DM6437 data sheet, I found that MCBSP0(not MCBSP1) is only used for the SPI boot mode.

Till now, I don't find any restriction to configure the  MCBSP1 as SPI device to interface with the FPGA.

however to confirm....   is it possible to configure both MCBSP's to be used as SPI  interfaces.?? or any restriction for the same?

thanks & regars,

Sri