Other Parts Discussed in Thread: ADS1626, TL16C550C
the circuit system works with DSK6416 and ADS1626EVM. And two EDMA channels are used with a ping pang buffering to collect AD data. Other EDMA channel is used to send out the result data with UART bulit with TL16C550C. And both ADS1626 and TL16C550 connect to DSP with EMIF. However, the EDMA channels for ADS1616EVM couldn't work together properly with the EDMA channel for TL16C550C, on the contrary both of the single part can separately work properly. Also I have set the priorities of the both EDMA. Could you give me some advice, Thanks a lot.