Part Number: AM68
Tool/software:
Hi,
I have some code I want to load in the external SDRAM and copy to DSP L2 at boot and run from there. I'm struggling to follow the documentation to get this working.
So far I have:
SECTIONS
{
...
.l2_code: load > __CORE_DDR_SPACE, run > __CORE_L2_SPACE
}
and .l2_code is done with a PRAGMA;
#define CODE_SECTION_INT PRAGMA(SET_CODE_SECTION(".l2_code"))
which I place before the various functions I want in .l2_code.
So in the map I get:
.l2_code 0 0000a6528240 00003400 RUN ADDR = 000064810000
0000a6528240 00000f80 input.obj (.l2_code)
0000a65291c0 00000d80 process.obj (.l2_code)
0000a6529f40 00000940 effect.obj (.l2_code)
...
which looks good, but now I can't figure out how or where to make a copy table which will move the .l2_code section from __CORE_DDR_SPACE to __CORE_L2_SPACE at boot.
Can you show me what needs to happen to move the code at boot?
Thanks,
Matt