Part Number: AM6442
Tool/software:
I’m evaluating the AM6442 (AM64x family) for a project that requires strict compliance with certain TSN standards. I have reviewed the datasheet, SDK release notes (SPRT769), and driver documentation, but I could not find explicit confirmation on whether the following are hardware- or firmware-supported for AM6442:
- IEEE 802.1CB — Frame Replication & Elimination for Reliability
- IEEE 802.1AE — MACsec (Media Access Control Security)
- IEEE 802.1Qci — Per-Stream Filtering & Policing
Specifically, could you clarify:
- If AM6442 supports these standards in silicon / hardware accelerators, or whether they must be implemented in software / firmware (e.g. via PRU-ICSSG).
- If there are any example driver stacks, SDK versions, or EVM demonstrations showing these features.
- If support for any of these is planned (roadmap) if not currently available.
Thanks very much for your assistance.