This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems with DSI configuration

Hi everyone,

we are developing our own platform based on omap4430 and we faced some problems while configuring DSI driver (dsi.c file) in kernel (Android L27.G.3). In dsi_videomode_panel_preinit function DSI_VM_TIMINGx registers are modified. How are the values 'HBP', 'HFP', 'HSA' calculated? These .dsi_video_timings are set in LCD driver (panel-d2l.c) and looks like they derive from  'D2L timings' - parameters set in panel-d2l.h and used by dispc. I'd like to use the values that fit best for our LCD, but timing calculation is not decribed in any documentation...

Best regards,

Marcin

  • Alot of the time, those values are given in the manufacturer's documentation. In general for DSI, the porch times have a wide range values which will work. I will typically split however many clock cycles are left from a horizonal or vertical sweep between the two.

    Regards,

    Matt

  • Thank you for the answer. Of course LCD manufacturer gives us the parameters' values expressed in the number of pixels, but DSI_VM_TIMING1 and DSI_VM_TIMING3 registers require the same thing described by number of byte clock cycles (TXBYTECLKHS clock). The dispc driver needs the number of pixels and dsi driver needs the number of clock cycles- yet they are hardcoded for blaze tablet lcd and changing them disrupts communication. To be clear- what we are asking for is the formula/dependancies that would enable calculation the number of TXBYTECLKHS cycles basing on the number of pixels in line, horizontal front porch, back porch and puls width.

    Best regards, 

    Marcin

  • Can you provide some more specfic information? What is the size of the panel, what refresh rate. How many data lanes are you using? What pixel clk does the manufacturer require?

    TXBYTECLKHS is CLKIN4DDR/16.

    Matt

  • Our parameters for DSI (panel-d2l.c). 

    WIDTH		1280
    HEIGHT 800
    PCLK 65183
    HFP 282
    HSW 6
    HBP 32
    VFP 15
    VSW 8
    VBP 15

    Because of hardcoding (except for width and height) we used blaze tablet settings. We managed however to enable SoC-D2L-LCD link and view the images from frame buffer on LCD. Nevertheless we faced another problem while using the bridge – its description is presented below.

    Our setup :
    LCD :    AUO B101EW05 V1 (1280x800@60Hz, RGB666, 3 data + 1 clock LVDS lanes, pixel clock required 64 - 85MHz)
    D2L :    TC358765XBG (EXTCLK for the bridge is taken from FREF_CLK4 @38,4MHz - multiplied by bridge internal PLL to apropriate range)
    SoC :    OMAP4430 (DSI output: 4 data + 1 clock)

    The problem is that in single-link LVDS mode the image on LCD screen indicates huge instability (most of the lines flicker randomly, therefore anything else is barely visible). It is clear and stable only in dual-link LVDS mode (LVDLINK bit set to '1' in LVCFG register). This situation would be acceptable, if there wasn't one fault- the bridge sends 2 pixels during one clock cycle on both links simultaneously, hence the even pixels are missed and the odd ones are doubled on LCD- the effect is that we have only a half of the horizontal resolution.

    Unfortunately we couldn't resolve this issue basing on OMAP4 and TC358765XBG documentation. Did you have similar problems with blaze tablet LCD configuration? Do you have any additional documentation for DISPC/DSI/D2L configuration? Does it make any difference for OMAP4 if there is single- or dual-link LVDS mode used in bridge?

    Regards,

    Marcin 

  • Marcin,

    i've been trying to research and document this info as well. please post any findings you get here!

    Dave

  • Matthew,

    for reference we can look at this panel config and pandaboard :

    https://gitorious.org/~boddob/linux-omap-dss2/archit-dss2-clone/blobs/lg-panel-work/drivers/video/omap2/displays/panel-lg4591.c#line44

    https://gitorious.org/~boddob/linux-omap-dss2/archit-dss2-clone/blobs/lg-panel-work/arch/arm/mach-omap2/board-omap4panda.c#line660

    Dave

  • Hi Marcin,

    There are quite some restrictions to these values.

    You can take a look on this patch: thttp://review.omapzoom.org/#/c/16063/

    This patch is for K3.0 (Icescream), not sure if it is ported for older kernels but you could get the idea.

    Basically you determine DISPC timings based on your panel specs. Then, DSI timings are on terms of TXBYTECLK while DISPC are on terms of PIXEL CLK. Having the relation between these two clocks you could have an estimate of what DSI timings should be, however there are some tricky restrictions there.

    DSI should be based on DISPC, but since DSI can buffer a line (or two), it can use their own timings as long as it is still with sync with the DISPC.

    Let me know if you have more particular questions after giving it a look at the patch.

    Regards,

    Jorge Bustamante