Other Parts Discussed in Thread: M2-CC3351, CC3351, AM625
Tool/software:
Hi,
I’m currently working with the following setup:
-
PSDK Version: ti-processor-sdk-linux-am62pxx-evm-10.01.10.04
-
Board: SK-AM62Px-LP
-
Audio Codec Module: TLV320AIC3106IRGZT
-
Bluetooth Module: EAR00388 (as recommended in the AM62Px User Guide, M.2 module)
I am trying to implement an audio system using Bluetooth. When I play a song from a mobile device, the audio is received, but only noise is heard through the headset jack. However, when I play a stored song sample rate (44.1 kHz, 16-bit), the sound is clear. The issue occurs only with Bluetooth playback, where noise is present instead of clear audio. The Bluetooth song sample rate is also the same
Could you please advise how to fix this issue?
Regards,
Veerapandiyan V.