AM62L: Proper connection to use debugger on customer board

Part Number: AM62L

Tool/software:

Hi, 

Assigned focus customer asks:

On the EVB, it seems like we can debug using the XDS110 debugger or we can use the cTI 20-pin JTAG connector. For our board, we will have test points for the JTAG signals, and we will have an adaptor board that connects to these JTAG signals and will be used for debugging. 

We would like to avoid the added complexity of using the XDS110 debugger, by using the cTI 20-pin JTAG connector. If we do this, would we just use a Jlink to connect from our PC to the cTI 20-pin header?

Pretty sure the answer is 'yes - just use the 20 pin connector - but are there any additional steps?  Any passives to add?'

Thanks!

Blake