This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6713B: CVDD Power Supply Requirement

Part Number: TMS320C6713B
Other Parts Discussed in Thread: TPS54310, , TPS62130, TPS62813M, TPS62813-Q1

Tool/software:

Hi team,

My customer is considering the TPS54310 because it is used in the TMS320C6713B EVM.
However, I'm concerned that it is an old device.
Vin is 3.3 V, Vout is 1.4 V (CVDD). Could you recommend a suitable replacement?
The customer is currently looking at the TPS62130 and TPS62813M; are these acceptable?

Here's the suggestion from SR team.

 TPS54310: TPS54310 Recommended Successor 

But they recommend to double check with DSP team.

Best regards,
Kazuki Itoh

  • Hello Kazuki Itoh

    Thank you for the query.

    Based on the current requirements including margin, TPS62813-Q1 can be an option that can be considered.

    There is a 4A part also in the family.

    The recommendation is to perform some quick tests in case customer has a option to test.

    Regards,

    Sreenivasa