This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62P: Enabling uart_callback mode in WKUP domain

Part Number: AM62P

Tool/software:

Hi,

I am trying to enable the uart_callback mode in WKUP domain but I found that there is no example projects for this. So I created an empty WKUP project and copied the "uart_echo_callback.c" to this project. The uart channel I selected is WKUP_UART0, I found the program is blocked at line 50 and the breakpoint cannot be inserted in the function "uart_echo_write_callback" . I just want to doublecheck whether the uart_callback mode in WKUP domain is feasible or this phenomenon is caused my coding mistakes.

I attached the relevant code and figures below.

BR,

Bomiao

#include <string.h>
#include <kernel/dpl/DebugP.h>
#include "ti_drivers_config.h"
#include "ti_drivers_open_close.h"
#include "ti_board_open_close.h"

#define APP_UART_BUFSIZE              (200U)
#define APP_UART_RECEIVE_BUFSIZE      (8U)

uint8_t gUartBuffer[APP_UART_BUFSIZE];
uint8_t gUartReceiveBuffer[APP_UART_RECEIVE_BUFSIZE];
volatile uint32_t gNumBytesRead = 0U, gNumBytesWritten = 0U;

/* Semaphore to indicate Write/Read completion used in callback api's */
static SemaphoreP_Object gUartWriteDoneSem;
static SemaphoreP_Object gUartReadDoneSem;

#define APP_UART_ASSERT_ON_FAILURE(transferOK, transaction) \
    do { \
        if((SystemP_SUCCESS != (transferOK)) || (UART_TRANSFER_STATUS_SUCCESS != transaction.status)) \
        { \
            DebugP_assert(FALSE); /* UART TX/RX failed!! */ \
        } \
    } while(0) \

void uart_echo_callback(void *args)
{
    int32_t          transferOK, status;
    UART_Transaction trans;

    DebugP_log("[UART] Echo callback example started ...\r\n");

    status = SemaphoreP_constructBinary(&gUartWriteDoneSem, 0);
    DebugP_assert(SystemP_SUCCESS == status);

    status = SemaphoreP_constructBinary(&gUartReadDoneSem, 0);
    DebugP_assert(SystemP_SUCCESS == status);

    UART_Transaction_init(&trans);

    /* Send entry string */
    gNumBytesWritten = 0U;
    trans.buf   = &gUartBuffer[0U];
    strncpy(trans.buf,"This is uart echo test callback mode\r\nReceives 8 characters then echo's back. Please input..\r\n", APP_UART_BUFSIZE);
    trans.count = strlen(trans.buf);
    transferOK = UART_write(gUartHandle[CONFIG_UART_CONSOLE], &trans);
    APP_UART_ASSERT_ON_FAILURE(transferOK, trans);

    /* Wait for write completion */
    SemaphoreP_pend(&gUartWriteDoneSem, SystemP_WAIT_FOREVER);
    DebugP_assert(gNumBytesWritten == strlen(trans.buf));

    /* Read 8 chars */
    gNumBytesRead = 0U;
    trans.buf   = &gUartReceiveBuffer[0U];
    trans.count = APP_UART_RECEIVE_BUFSIZE;
    transferOK = UART_read(gUartHandle[CONFIG_UART_CONSOLE], &trans);
    APP_UART_ASSERT_ON_FAILURE(transferOK, trans);

    /* Wait for read completion */
    SemaphoreP_pend(&gUartReadDoneSem, SystemP_WAIT_FOREVER);
    DebugP_assert(gNumBytesRead == APP_UART_RECEIVE_BUFSIZE);

    /* Echo chars entered */
    gNumBytesWritten = 0U;
    trans.buf   = &gUartReceiveBuffer[0U];
    trans.count = APP_UART_RECEIVE_BUFSIZE;
    transferOK = UART_write(gUartHandle[CONFIG_UART_CONSOLE], &trans);
    APP_UART_ASSERT_ON_FAILURE(transferOK, trans);

    /* Wait for write completion */
    SemaphoreP_pend(&gUartWriteDoneSem, SystemP_WAIT_FOREVER);
    DebugP_assert(gNumBytesWritten == APP_UART_RECEIVE_BUFSIZE);

    /* Send exit string */
    gNumBytesWritten = 0U;
    trans.buf   = &gUartBuffer[0U];
    strncpy(trans.buf, "\r\nAll tests have passed!!\r\n", APP_UART_BUFSIZE);
    trans.count = strlen(trans.buf);
    transferOK = UART_write(gUartHandle[CONFIG_UART_CONSOLE], &trans);
    APP_UART_ASSERT_ON_FAILURE(transferOK, trans);

    /* Wait for write completion */
    SemaphoreP_pend(&gUartWriteDoneSem, SystemP_WAIT_FOREVER);
    DebugP_assert(gNumBytesWritten == strlen(trans.buf));

    SemaphoreP_destruct(&gUartWriteDoneSem);
    SemaphoreP_destruct(&gUartReadDoneSem);

    DebugP_log("All tests have passed!!\r\n");

    return;
}

void uart_echo_write_callback(UART_Handle handle, UART_Transaction *trans)
{
    DebugP_assertNoLog(UART_TRANSFER_STATUS_SUCCESS == trans->status);
    gNumBytesWritten = trans->count;
    SemaphoreP_post(&gUartWriteDoneSem);

    return;
}

void uart_echo_read_callback(UART_Handle handle, UART_Transaction *trans)
{
    DebugP_assertNoLog(UART_TRANSFER_STATUS_SUCCESS == trans->status);
    gNumBytesRead = trans->count;
    SemaphoreP_post(&gUartReadDoneSem);

    return;
}

  • Hi,

    Please refer this FAQ to understand the usage of different UART ports: e2e.ti.com/.../4839735

    Before starting with echo callback, please verify the normal uart echo working with wkup example + wkup uart0

    Please see if your able to input characters onto the console for the blocking echo example, then we can look at the callback implementation.

    Additionally please refer this: software-dl.ti.com/.../DEVELOP_AND_DEBUG_DMR5.html

    Thanks,

    Vaibhav

  • Hi,

    Now I am trying to test the example project "uart_echo_callback_am62px-sk_mcu-r5fss0-0_freertos_ti-arm-clang". I have noticed the code introduces "SemaphoreP_Object" to monitor the transfer status of UART Write/Read. When I commented the codes related to Semaphores, I found that the project cannot run normally and it reports "UART Write failed". I wonder whether we could discard those Semaphores because I think Semaphores is just a bonus to monitor the transfer process and the code should run normally without Semaphores .

    I attached my code below.

    #include <string.h>
    #include <kernel/dpl/DebugP.h>
    #include "ti_drivers_config.h"
    #include "ti_drivers_open_close.h"
    #include "ti_board_open_close.h"
    
    #define APP_UART_BUFSIZE              (200U)
    #define APP_UART_RECEIVE_BUFSIZE      (8U)
    
    uint8_t gUartBuffer[APP_UART_BUFSIZE];
    uint8_t gUartReceiveBuffer[APP_UART_RECEIVE_BUFSIZE];
    volatile uint32_t gNumBytesRead = 0U, gNumBytesWritten = 0U;
    
    /* Semaphore to indicate Write/Read completion used in callback api's */
    // static SemaphoreP_Object gUartWriteDoneSem;
    // static SemaphoreP_Object gUartReadDoneSem;
    
    #define APP_UART_ASSERT_ON_FAILURE(transferOK, transaction) \
        do { \
            if((SystemP_SUCCESS != (transferOK)) || (UART_TRANSFER_STATUS_SUCCESS != transaction.status)) \
            { \
                DebugP_assert(FALSE); /* UART TX/RX failed!! */ \
            } \
        } while(0) \
    
    void uart_echo_callback(void *args)
    {
        int32_t          transferOK, status;
        UART_Transaction trans;
    
        DebugP_log("[UART] Echo callback example started ...\r\n");
    
        // status = SemaphoreP_constructBinary(&gUartWriteDoneSem, 0);
        // DebugP_assert(SystemP_SUCCESS == status);
    
        // status = SemaphoreP_constructBinary(&gUartReadDoneSem, 0);
        // DebugP_assert(SystemP_SUCCESS == status);
    
        UART_Transaction_init(&trans);
    
        /* Send entry string */
        gNumBytesWritten = 0U;
        trans.buf   = &gUartBuffer[0U];
        strncpy(trans.buf,"This is uart echo test callback mode\r\nReceives 8 characters then echo's back. Please input..\r\n", APP_UART_BUFSIZE);
        trans.count = strlen(trans.buf);
        transferOK = UART_write(gUartHandle[CONFIG_UART_CONSOLE], &trans);
        APP_UART_ASSERT_ON_FAILURE(transferOK, trans);
    
        /* Wait for write completion */
        // SemaphoreP_pend(&gUartWriteDoneSem, SystemP_WAIT_FOREVER);
        // DebugP_assert(gNumBytesWritten == strlen(trans.buf));
    
        /* Read 8 chars */
        gNumBytesRead = 0U;
        trans.buf   = &gUartReceiveBuffer[0U];
        trans.count = APP_UART_RECEIVE_BUFSIZE;
        transferOK = UART_read(gUartHandle[CONFIG_UART_CONSOLE], &trans);
        APP_UART_ASSERT_ON_FAILURE(transferOK, trans);
    
        /* Wait for read completion */
        // SemaphoreP_pend(&gUartReadDoneSem, SystemP_WAIT_FOREVER);
        // DebugP_assert(gNumBytesRead == APP_UART_RECEIVE_BUFSIZE);
    
        /* Echo chars entered */
        gNumBytesWritten = 0U;
        trans.buf   = &gUartReceiveBuffer[0U];
        trans.count = APP_UART_RECEIVE_BUFSIZE;
        transferOK = UART_write(gUartHandle[CONFIG_UART_CONSOLE], &trans);
        APP_UART_ASSERT_ON_FAILURE(transferOK, trans);
    
        /* Wait for write completion */
        // SemaphoreP_pend(&gUartWriteDoneSem, SystemP_WAIT_FOREVER);
        // DebugP_assert(gNumBytesWritten == APP_UART_RECEIVE_BUFSIZE);
    
        /* Send exit string */
        gNumBytesWritten = 0U;
        trans.buf   = &gUartBuffer[0U];
        strncpy(trans.buf, "\r\nAll tests have passed!!\r\n", APP_UART_BUFSIZE);
        trans.count = strlen(trans.buf);
        transferOK = UART_write(gUartHandle[CONFIG_UART_CONSOLE], &trans);
        APP_UART_ASSERT_ON_FAILURE(transferOK, trans);
    
        /* Wait for write completion */
        // SemaphoreP_pend(&gUartWriteDoneSem, SystemP_WAIT_FOREVER);
        // DebugP_assert(gNumBytesWritten == strlen(trans.buf));
    
        // SemaphoreP_destruct(&gUartWriteDoneSem);
        // SemaphoreP_destruct(&gUartReadDoneSem);
    
        DebugP_log("All tests have passed!!\r\n");
    
        return;
    }
    
    void uart_echo_write_callback(UART_Handle handle, UART_Transaction *trans)
    {
        DebugP_assertNoLog(UART_TRANSFER_STATUS_SUCCESS == trans->status);
        gNumBytesWritten = trans->count;
        //SemaphoreP_post(&gUartWriteDoneSem);
    
        return;
    }
    
    void uart_echo_read_callback(UART_Handle handle, UART_Transaction *trans)
    {
        DebugP_assertNoLog(UART_TRANSFER_STATUS_SUCCESS == trans->status);
        gNumBytesRead = trans->count;
        //SemaphoreP_post(&gUartReadDoneSem);
    
        return;
    }

    BR,

    Bomiao

  • Hi Bomiao,

    I tested out WKUP UART in blocking mode and it worked out for me.

    For callback mode, I am seeing issues as well. If you have any update on this since your last experiment, do let me know.

    I have raised an internal bug for the same.

    Thanks,

    Vaibhav