Part Number: TDA4VH-Q1
Tool/software:
Hello TI Expert,
We want to send canfd data with BRS.
We tried sending canfd data from terminal with & without brs bit enabled, and the data was transmitted to CANoe if sent with brs disabled & was not when brs is enabled.
without brs enabled: cansend main_mcan12 123##0deadbeef -> data received in CANoe successfully
with brs enabled: cansend main_mcan12 123##1deadbeef -> throws Stuff error with bit position
So, can you please tell if there's anything needed to be changed for BRS in the CANoe config side or driver side.
Note: We also set the config as follows before sending the command:
ip link set main_mcan12 type can bitrate 500000 dbitrate 4000000 fd on
ip link set main_mcan12 up
Thanks & Regards,
Syed Fawwaz.