This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to encode via HDMI input port ?

Hi all,

At my DM8168 board,

I want to achieve the flow below:

HDMI Video Input => DM8168 encoder(*1) => h264 file

*1: encoder like omtb_dm816xbm_a8host.xv5T
    I use ezsdk of ti-ezsdk_dm816x-evm_5_03_01_15

With best regards,

-- M.Nakayama

  • Hi,

    Which is the expansion card are you using. HDMI encoders is not present on IO expansion card. HDMI connector present on IO expansion card is for DVI capture. Which is done using SII1161. We dont have driver for SII1161 as of now.

    Regards,

    Hardik Shah

  • Hi,

    Thank you for your reply.

    I understood that HDMI encoders of DM8168 is not present on IO expansion card.

    With best regards,

    --M.Nakayama

     

     

  • Hi,

    Thank you for your reply.

    I add a postscript to the question.

    How to capture for DVI ?

    I want to achieve the flow below:

    DVI Video Input (HDMI connector)  ->  DM8168 encoder(*1)  -> h.264 file

    (*1) encoder like omtb_dm816xbm_a8host.xv5T

           I use ezsdk of ti-exsdk_dm816x-evm_5_03_01_15

          ex. DVI Video Input is HD camera Input.

    With best regards,

    --M.Nakayama