This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AUDIO-AM62D-EVM: SDK 11.01.16.06, app_a53 is different in supplied BIN folders for CFG2 vs CFG3

Part Number: AUDIO-AM62D-EVM
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

I haven't seen any problem due to this but am just curious.  When I do a "gmake" to build the BSP for all cores, there's no consideration as far as I can tell as to which CFG is targeted.

When I connect to AWE Server, both A53 instances show AWECore version 8.C.0.7 and build number 2399.

app_a53 in the cfg2 folder is 1014 KB

app_a53 in the cfg3 folder is 953 KB

Does anyone know the reason for this discrepancy?  I'm assuming that when I build for all cores using "gmake" that I don't have to do anything special for the a53 regardless of which cfg I wish to use.

Thanks,

GW