Part Number: SK-TDA4VM
Tool/software:
Hi,
I was trying to generate traces for a DL model on the SK-TDA4VM, but the execution hangs and I have to kill the process.
To make sure the problem is not related to my script, I ran
/opt/edgeai-tidl-tools/examples/osrt_python/ort# python3 onnxrt_ep.py -m cl-ort-resnet18-v1
and changed debug_level to 3 in /opt/edgeai-tidl-tools/examples/osrt_python/common_utils.py
This hangs too. Following is the output of the command
root@tda4vm-sk:/opt/edgeai-tidl-tools/examples/osrt_python/ort# python3 onnxrt_ep.py -m cl-ort-resnet18-v1 Available execution providers : ['TIDLExecutionProvider', 'TIDLCompilationProvider', 'CPUExecutionProvider'] Running 1 Models - ['cl-ort-resnet18-v1'] Running_Model : cl-ort-resnet18-v1 libtidl_onnxrt_EP loaded 0x1246f120 artifacts_folder = ../../../model-artifacts//cl-ort-resnet18-v1/artifacts debug_level = 3 target_priority = 0 max_pre_empt_delay = 340282346638528859811704183484516925440.000000 Final number of subgraphs created are : 1, - Offloaded Nodes - 52, Total Nodes - 52 In TIDL_createStateInfer Compute on node : TIDLExecutionProvider_TIDL_0_0 ************ in TIDL_subgraphRtCreate ************ APP: Init ... !!! 1013.725896 s: MEM: Init ... !!! 1013.725943 s: MEM: Initialized DMA HEAP (fd=5) !!! 1013.726091 s: MEM: Init ... Done !!! 1013.726114 s: IPC: Init ... !!! 1013.783908 s: IPC: Init ... Done !!! REMOTE_SERVICE: Init ... !!! REMOTE_SERVICE: Init ... Done !!! 1013.790888 s: GTC Frequency = 200 MHz APP: Init ... Done !!! 1013.790988 s: VX_ZONE_INFO: Globally Enabled VX_ZONE_ERROR 1013.790999 s: VX_ZONE_INFO: Globally Enabled VX_ZONE_WARNING 1013.791009 s: VX_ZONE_INFO: Globally Enabled VX_ZONE_INFO 1013.791544 s: VX_ZONE_INFO: [tivxPlatformCreateTargetId:169] Added target MPU-0 1013.791659 s: VX_ZONE_INFO: [tivxPlatformCreateTargetId:169] Added target MPU-1 1013.791760 s: VX_ZONE_INFO: [tivxPlatformCreateTargetId:169] Added target MPU-2 1013.791852 s: VX_ZONE_INFO: [tivxPlatformCreateTargetId:169] Added target MPU-3 1013.791865 s: VX_ZONE_INFO: [tivxInitLocal:202] Initialization Done !!! 1013.791881 s: VX_ZONE_INFO: Globally Disabled VX_ZONE_INFO ************ TIDL_subgraphRtCreate done ************ ******* In TIDL_subgraphRtInvoke ********
I need the traces to compare a mismatch between model run in host emulation mode inside docker with the model being run on the board.
I am following instructions given in the TIDL repo.
Thank you in advance,
Charanjit