Other Parts Discussed in Thread: CCSTUDIO
Tool/software:
Hello,
I'm trying to program the TMS320VC5510A with Spectrum digital XDS510 USB emulator.
I've installed ccstudio v3.3 and FlashBurn v3.11.
1. I cannot see TMS320VC5510A but only TMS320C5510 v1 or v2
2. I've tried selecting the TMS320C5510A v1 and also v2 but when I click on "save & quit", then the code composer is started and it always says "No Target connected".
If I click on "debug" -> "connect" I get the following error message:
Error connecting to the target:
Error 0x80000240/-141
Fatal Error during: Initialization, OCS,
This error was generated by TI's USCIF driver.
SC_ERR_KNL_OPEN <-141>
This utility has failed to open its kernel mode driver.
Either it has been disabled or an install/un-install failed.
What could be the problem?
Thanks in advance
Steve