AM62A7: The highlights are too white, and in strong sunlight, the image is almost entirely white.

Part Number: AM62A7

Tool/software:

Hi Ti Experts

My sensor is an OX03C10, configured to output 12-bit Raw images.
The current driver is a modified version of the IMX219 driver.

After applying WDR using a DCC tool, I hope to be able to see both highlights and shadows clearly.
Currently, the image is clear in low-light conditions.
However, there are two issues:
1: In conditions with strong contrast, the highlights appear completely white and overexposed.
2: The halo from car lights at night is too large and bright, making it difficult to reduce the halo.

Also: The X-axis of the WDR curve gradually transitions from low light, medium light, to high light. The Y-axis represents the brightness of the converted output. Am I understanding this correctly? However, during actual debugging, I set the brightness value for the medium-high light portion to the lowest and applied it to the camera program. This had little effect on the image (the image now included the transition from shadows to high light). Conversely, increasing or decreasing the Y value for the low-light portion significantly increased or decreased the image brightness.

Here is my pic file

7823.e2e.rar

Best Regards 

Meng