Tool/software:
Hi Team,
We have SK-AM62A-LP evk board, While trying to boot from sd-card,it shows unable to load uboot.img
when checked inside the boot partition of sd-card, u-boot.img, is present also we have build the image via yocto and evk is in sd card boot mode
Flashed the .wic img using etcher tool
target image - tisdk-edgeai-image
U-Boot SPL 2025.01-00547-g3bcfad6cee95 (Jul 23 2025 - 16:49:22 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000b '11.1.5--v11.01.05 (Fancy Rat)')
DM ABI: 3.0 (firmware ver 0x000b 'MSDK.11.01.00.16-dirty--v11.01.02' patch_ver: 2)
Trying to boot from MMC2
Error reading cluster
spl_load_image_fat: error reading image u-boot.img, err - -22
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
Any help would be appreciated