Part Number: 66AK2G12
Tool/software:
Hi experts,
My customer is experiencing an issue with a product that uses the 66AK2G12.
They are currently investigating to determine if the problem is with the K2G. -
- The USB0 port is used in the default HOST setting, but when an iPad app is connected, the power role remains HOST and the data role switches from HOST to Function.
- When this happens, audio noise is constantly mixed in (it's not that the connection itself is working and the sound is choppy, but rather that playback is occurring but there is constant noise superimposed on the audio).
- From past experience, this is similar to a case where the cable length is being checked (using an extended cable to a length that does not conform to the USB standard (6m)).
Please explain the differences between using USB0 as a normal HOST and using it with a data role swap and switching to Function.
Q1: Are there any registers that are common before and after a data role swap, or registers whose references change depending on the data role?
Q2:Are there any areas where this symptom is likely to occur if register settings are not configured correctly when swapping data roles?
Best regards,
O.H