Part Number: CCSTUDIO
Other Parts Discussed in Thread: CC1312R7, SYSCONFIG
Tool/software:
Hello Technical Support Specialist,
I'm encountering an issue while trying to build and flash the Wi-SUN ns_br example to my CC1312R7 board.
Initially, I attempted this on my MacBook M3 running macOS Sonoma 14.1. However, the project fails to run and displays the message:
"Autorun: Target not run as symbol 'main' is not defined."
Since I was stuck and couldn't resolve the issue, I switched to a headless Linux machine and successfully built and flashed the firmware using the command line. Everything worked smoothly there.
Now, I want to modify the PHY settings using the SysConfig tool. As you've mentioned in earlier support threads, it's not possible to change PHY settings without SysConfig. Unfortunately, SysConfig doesn't run on headless Linux systems.
So I'm back on my MacBook, but the same issue persists.
In another support thread, it was suggested to downgrade to version 3.2.2 of the tiarmclang compiler. Interestingly, I didn't use that version on the Linux machine, and it still worked fine.
Nevertheless, I tried downgrading to version 3.2.2 on my MacBook as recommended, but the problem remains.

So the question is:
How to fix this:
1) By somewhow use sysconfigtool on headless Linux (my prefered solution)
2) Or by solving the error message.
Can you give me any advise?
Regards
Elfred