AM6421: industria communication SDK11.00.00.13

Part Number: AM6421
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

Hi,

     We are using below

 Industrial Communication SDK :11.00.00.13

 CCS : 12.8.1

 SYSCONFIG : 1.22

Compiler : tiarmclang 4.0.1

After launching Target configuration and Script, we are getting below error.

MAIN_Cortex_R5_0_0: Trouble Writing Memory Block at 0x0 on Page 0 of Length 0x1378: (Error -1065 @ 0x1000) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 20.0.0.3178)
MAIN_Cortex_R5_0_0: File Loader: Verification failed: Target failed to write 0x00000000

Please guide to resolve this issue.

Same application is working with indistrial SDK 9.02.00.24 and CCS 12.7.1 and Sysconfig : 1.20.0

also we are getting below error in CIO console.

[MAIN_Cortex_R5_0_0]
DMSC Firmware Version 11.0.6--v11.00.06 (Fancy Rat)
DMSC Firmware revision 0xb
DMSC ABI revision 4.0

[SCICLIENT] ABI check PASSED
[SCICLIENT] Board Configuration with Debug enabled ...
[SCICLIENT] Common Board Configuration PASSED
[SCICLIENT] PM Board Configuration PASSED
[SCICLIENT] RM Board Configuration PASSED
[SCICLIENT] Security Board Configuration PASSED

DMSC Firmware Version 11.0.6--v11.00.06 (Fancy Rat)
DMSC Firmware revision 0xb
DMSC ABI revision 4.0

Starting SOC Initialization ...
ERROR: Bootloader_socCpuResetRelease:873: CPU power on failed for a530-1
Resetting self cluster ...