This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with ethernet communication on TMS320DM642.

Other Parts Discussed in Thread: TMS320DM642

I am a beginner working on TMS320DM642 processor. I am having problem with the ethernet communcation using NDK stack.Sometimes the packets are getting dropped when more than 10-15 packets come at a time. I need UDP as well as TCP/IP for file transfer. Can anybody share the information on etherner driver and how to configure it? I need 100 Mbps ethernet.

  • Snehal,

    Are you looking to migrate to the StarterWare Ethernet stack, or do you want help getting the NDK to work?  If it's the latter, I recommend posting in the BIOS forum so you can get in touch with the NDK experts.

    StarterWare does offer a lightweight Ethernet stack based on the open source lwIP project.  However, the DM642 device is not supported by any StarterWare release.  For more information about StarterWare and supported devices, please refer to the StarterWare wiki page.